OMRON TECHNICS -Technical Papers-
This webpage introduces technical papers that describe the outcomes of the OMRON Group’s R&D activities, as well as the technologies that support its products and services.
-
The importance of data utilization in manufacturing has rapidly increased in recent years. Factory automation (FA) systems are shifting from control-centric to data-centric architectures driven by advances in IoT, AI, and cloud technologies. This paper presents OMRON’s proof-of-concept (PoC) implementation, which verified six use cases: ...
- Digital Twin
- AAS
- OPC UA
- Carbon Footprint
-
Manual assembly lines are required to improve not only productivity but also energy efficiency. In manufacturing sites, improvement activities are being conducted to address variations in the 4M factors—Man (operator), Machine (equipment), Material, and Method. However, in cell production systems (cell lines), ...
- Production Technology
- Manual Work
- Assembly Line
- Electric power Simulation
- Cell Line
-
This paper presents a refinement of obstacle constraints in trajectory planning for autonomous mobile robots using Model Predictive Control (MPC). MPC generates velocity commands that guide the robot to achieve a given goal by adjusting its position and orientation over time. In MPC formulations, obstacle constraints ...
- Trajectory Planning
- Optimization
- Robotics
-
The quality of traffic signal control is directly linked to such social issues as traffic jams and environmental issues. In the past, skilled engineers have maintained and improved this quality. For signal control, we need to adjust the signals with neighboring ones. ...
- Traffic Signal Control
- Reinforcement Learning
- Traffic Engineering
- Subarea Control
- AI Technology
-
Blood pressure management is important for preventing cerebrovascular and cardiovascular diseases, but it is not being adequately achieved and has become a global social issue. In the United States, public and private initiatives have tried various solutions. Insurance made remote patient ...
- Telemonitoring
- Remote Patient Monitoring
- Hypertension Treatment
- Hypertension Control
- Blood Pressure Monitor
-
In modern manufacturing, labor shortages due to population decline have increased the need for further automation. Additionally, to respond to diversifying needs and rapid technological innovation, highly flexible automated production is essential. This requires sensors that can reliably detect objects from long distances without obstructing ...
- TOF Laser Sensor
- dTOF
- High-speed laser driver circuit
- APD individual variation correction
- APD temperature compensation
-
In the NJ and NX series of OMRON’s machine automation controllers, the internal central processing unit (CPU) and the internal devices are connected using PCI Express (PCIe). One of the features of PCIe is that it allows direct memory access (DMA) to execute the data transfer without going through the CPU. ...
- PLC
- Real Time System
- PCI Express
- Time Synchronization
- DMA
-
Today, in-factory logistics faces the social challenge of labor shortages while the importance of parts management increases. To address this, automation aimed at reducing human labor is being implemented, and there is a demand for advanced material and parts management system functions on-site. ...
- UHF RFID
- Estimation Algorithm
- Traceability
- Luggage Management
- Automation
-
Traditionally, electrocardiograms (ECG) have mainly employed the use of 12-lead ECG or Holter monitors in the medical field. However, depending on the patient, symptoms do not always appear on the waveform, and there are some patients whose symptoms cannot be detected by recording for a few seconds ...
- Electrocardiograph
- Portable
- Home
- Chassis
- Contact Resistance
-
In recent years, deep learning algorithms have been applied to sensing and are contributing to the enhancement of high-precision devices, such as image sensors. This study aims to apply deep learning algorithms to simple sensors that handle one-dimensional signals with the goal of improving accuracy ...
- Embedded device
- AI Technology
-
2025/08/25
Development of Middleware for Rapid Prototyping of Robots Based on Parallel Behavior Architecture
To realize robots that can move flexibly in human environments and automate nonstandard tasks, it is essential to parallel process functions like recognition, planning, and control to enhance responsiveness. The parallel behavior architecture addresses this requirement by executing high-level ...- Robot Middleware
- Robot System
- Real-time Control
- Parallel Processing
- Rapid Prototyping
-
It is crucial to utilize an intelligent transport system that gathers vehicle information from sensors installed as part of the road traffic infrastructure and uses this data for signal control and support for autonomous driving to ensure safe and smooth traffic flow control. ...
- Millimeter-wave radar
- Millimeter-wave radar food
- ITS (Intelligent Transport Systems)
- Snow accretion test
- Vehicle detection
-
As an adhesive for bonding dissimilar materials used in mechanical devices, one-component epoxy resins are widely used from the viewpoint of high strength and ease of use. We have also used one-component epoxy resins for mechanical devices, such as relays and switches. ...
- One Part Epoxy Resin
- Thermal analysis
-
Critical chain project management (CCPM) is one of the representative project management methods characterized by completing projects efficiently and on time through buffer management. However, when applying CCPM to research and development (R&D) projects with high variability and uncertainty,...
- Project Management
- Buffer Management
- CCPM
- Uncertainty in projects
- R&D
-
In order to meet the diversifying needs of today’s consumers, there is a growing effort to realize variable-type, variable-volume production at a cost no less than that of mass production. To this end, it is necessary to shorten the tact time and start-up time for individual manufacturing equipment. ...
- Control Engineering
- Gain Tuning
- Servo Driver
- Frequency Response Analysis
- Simulation
-
In recent years, product lifespans have become shorter because of technological innovation, and it requires manufacturing facility to quickly support new product types. In response to this request, design information of products and manufacturing facilities are comprehensively managed using the Product Lifecycle Management (PLM) information platform, ...
- PLC
- Manufacturing Process Design
- PLM
- 3D Simulation
- Program Generation
-
In recent years, with the trend of machine learning, there has been an increase in the application of anomaly detection using machine learning to predict product defects in Factory Automation (FA) domain. However, because of the diversification of products and the efficiency of the manufacturing processes, ...
- Abnormal Detection
- Concept Drift
- Causal Relationship
- Machine Learning
-
2025/02/21
Realization to Achieve Both Standardization and Customization with Open Standards (OPC UA, PackML)
In recent years, many efforts have been made to increase productivity by standardizing manufacturing data (information) and unifying the design and maintenance in the manufacturing industry. On the other hand, customization (unique specifications or vendor-specific specifications) to create value and strengthen competitive advantage is ...- Information standardization
- Customization
- OPC UA
- PackML
- Controller
-
In recent years, production factories are required to identify the productivity bottlenecks and factors to respond to the diversification of production variety and/or worker turnover. An analysis of bottlenecks requires not only equipment operation data but also work time. However, the method for ...
- Industrial Engineering
- Productivity improvement
- Worktime measurement
- Human sensing technology
- Image processing
-
In recent years, the domestic semiconductor industry has faced intense competition and supply chain disruptions due to semiconductor shortages. Amid the phaseout of ASIC production using older processes, we have struggled with how to respond when ASIC production is discontinued to maintain product supply to customers. ...
- ASIC
- End of Life
- Remake
- Asynchronous Circuit
- PLC
-
In various fields, including medical and health management, the demand for vital sensing technology is increasing because of the proliferation of related services. One of them, millimeter-wave radar, is seen as a promising technology that can simultaneously measure the vital signs of multiple people in a noncontact manner with the body. ...
- Radar
- Vital measurement
- Clustering
- Respiratory rate
- Time series
-
Products are required to have robust quality to operate stably against disturbances in various usage environments. To satisfy such requirements, it is necessary to verify operation under a variety of different conditions and to eliminate conditions that cause unstable operation, which is where CAE ...
- System Simulation
- Causal Model
- CAE Application Technology
- Adaptive Design of Experiments
- Range Estimation Method
-
Defects that were not anticipated in the design stage may occur at the prototyping stage. One of the reasons for this is the variability that is difficult to control and observe in the experience. If the output value or its change characteristics are not constant due to the variation, the true mechanism ...
- Contact Analysis
- Thermal Stress Analysis
- Data Analysis
- Design Process
- Inverse problem approach
-
2024/12/10
Reduction of Waveform Discontinuity in Respiratory Waveform Measurement using Millimeter-Wave Radar
Human sensing, which measures human movements and vital signs, has become familiar to us with the proliferation of measurement devices and the expansion of related services. Among the various measurement devices, millimeter-wave radar has attracted much attention because it can accurately measure human ...- Millimeter-Wave Radar
- Vital Sensing
- Respiratory Waveform
- Discontinuity
- Waveform Analysis
-
2024/09/25
【Expository Articles】 Significance of Mass Balance Approach in the Dissemination of Biomass Plastics
In recent years, toward the realization of a carbon-neutral society, which is the Japanese government’s goal of achieving a carbon-neutral society by 2050, a movement to promote the spread of biomass plastics is becoming active. When switching from existing petroleum-derived plastics to biomass plastics, ...- Biomass Plastics
- Mass Balance Approach
- Carbon Neutral
- Circular Economy
- The Paris Agreement
-
In OMRON’s factory automation business, we provide solutions to address customer manufacturing issues by combining a rich product lineup and control algorithms. To expand this solution horizontally, we have built a technological knowledge sharing system and have made small improvements through DevOps, ...
- Information System
- Knowledge Management
- Information Architecture
- System Architecture
-
OMRON continues to take on the challenge of contributing to the spread of renewable energy equipment and high-speed communication equipment by providing devices and modules toward the realization of a carbon neutral and digitalized society. In order to realize these device performances, advanced ...
- Partial Plating
- Surface Treatment
- Metering liquid feeder
-
Amidst efforts for a carbon-neutral and decarbonized society, manufacturing automation speeds up because of the declining labor force and satellite factory promotion. The growing use of electric, safety, and IoT devices in manufacturing ...
- Power supply
- High-capacity
- Avoiding wiring burnout
- High efficiency
- Carbon neutral
-
Solving labor shortages and improving product quality are major issues at manufacturing sites, and artificial intelligence (AI) is being applied as a means of improvement. However, there are cases where it is difficult to apply conventional AI. ...
- AI technics
- Realtime anomaly detection
- Quality control
- PLC
- Machine learning algorithm
-
2024/01/11
Partial Discharge Voltage Prediction in Printed Wiring Boards and Their Expansion to High Frequency
With the recent increase in the frequency and power of power conversion equipment, the risk of dielectric breakdown in multilayer printed wiring boards is increasing. In order to respond to risks, a technology for predicting the partial discharge generation site and partial discharge starting voltage, including support for the high frequency range, has been desired. ...- Quality
- Partial Discharge
- Printed Wiring Board
- Power Electronics
- High Frequency
-
Millimeter-wave radars have been drawing interest as a means of contactless sensing of the positions of people and objects and are expected to be used in a wide range of fields, such as automotive, transportation infrastructure, factory automation (FA), and healthcare. In order for radars to correctly detect the position of the targets, it is necessary to estimate the direction of arrival of the radio waves with high accuracy. ...
- Millimeter-wave Radar
- Estimating Direction-of-arrival
- Waveguide
- SIW
- Suppressing Unnecessary Radiation
-
In order to inspect the solder joints of invisible components on increasingly sophisticated automotive electronic circuit boards, we have been providing automated X-ray inspection systems using the CT method. However, our conventional technology, VT-X750-V1/V2 with continuous image capture control, repeatedly stopped and moved the image capture system stage when moving it to the field of view to be inspected, resulting in a loss of acceleration and braking time. ...
- CT
- X-ray
- Automatic inspection system
- Inline
- Solder inspection
-
In recent years, rapidly changing market needs has led to a trend of shorter product lifecycles. To keep up with such market trends, it is necessary to shorten the launch time for production facilities. We introduced virtualization technology in our FA integrated development environment, Sysmac Studio, which enabled debugging without physical machines using a 3D simulation. ...
- Virtualization
- Integrated development environment
- Physics simulation
- PLC
- Mechanical device
-
The declining working population and the energy saving of production sites for decarbonization have become major social issues. Toward this end, methods to effectively utilize the regenerative power of motors have been proposed, and DC powering of servo drives is expected to achieve this. ...
- Power electronics
- EMI
- Conductive emission analysis
- Simulation
- Servo driver
-
Using deep learning technology, we searched for an alternative flame retardant coagent to antimony trioxide,which is a flame-retardant aid for polyester resins. Specifically, a deep learning model for physical property prediction was constructed based on the flame retardancy mechanism, and candidate materials were predicted andextracted. ...
- Polymers
- Flame retardant
- Deep learning
- Prediction of the characteristics
-
In preparation for responding to a recall when there is a defect in the product, it is necessary to quickly identify the recall target. In identifying the target, there is a method of assigning a 2D code that records traceability information such as the date of manufacture to the part. ...
- Laser marker
- Traceability
- 2D Code
- Galvano Scanner
- Takt Time
-
In OMRON’s factory automation business, engineers around the world provide effective technical solutions to address customer manufacturing issues, in order to bring more value to customers. For further acceleration, we built a system to formalize the technical know-how and to share and to utilize globally, which beforehand, remained within individual engineers or within each region. We setup and classified technological knowledge as the outcome ...
- Information System
- Knowledge Management
-
In mechanical devices such as relays and switches, polyester-based polymer molded products are used because of their excellent mechanical/electrical characteristics. On the other hand, it is important to control the dimensions of the molded product because the dimensions of the polyester-based polymer molded product change due to the application of heat. In this paper, we have found that coarsening of polymer crystal sizes is effective as a factor that ...
- Polymers
- High-order structure
- Dimensional stabilization
- Electronic components
- Evaluation technology
-
Recently, social interest in safety and security has increased, and in addition to quality improvement that does not bring defective products to the market, traceability to manage target parts and the manufacturing process is important for quick identification when defects occur. In addition, mainly in the automobile industry, problems of unreadable marking due to post-processes like heat/polishing and painting after marking on metal objects ...
- Traceability
- DPM
- Laser marker
- Fiber laser
- Marking quality
-
In recent years, labor force issues have become more serious, such as the declining labor force or the reduction in the number of skilled workers at manufacturing sites. And the factory automation necessity continues to increase as the countermeasure. In this paper, I propose a technique for defect classification using AI technology based on confirmation of the performance improvement compared with the conventional method. The conventional method ...
- AI Technology
- Deep Learning
- Auto Web Inspection System
- Defect Classification
-
In recent years with the trend toward IoT, there has been an increase in cases of causal analysis for product defects in the Factory Automation (FA) field. However, a conventional method is not effective because the collected data has low independence by multiple processes and synchronous control. To solve the issue, we focus on a PLC control program that has information of them. In this paper, we propose ...
- Program Slicing
- Mutual Information
- Causal Analysis
- Directed Graph
- PLC
-
2023/04/27
High Resolution Coaxial Displacement Sensor Using Small Diameter Fiber for Thickness Measurement
In in-line thickness inspection of glass and film for displays, there is a need for a sensor that is easy to adjust during installation and can stably measure even when tilted because of fluttering or wrinkling during transport. A fiber coaxial displacement sensor based on the chromatic confocal method has been released that replaces the triangulation distance measurement method that has been the mainstay of displacement sensors. The fiber coaxial displacement sensor is resistant to inclination on glossy surfaces, which has been a problem ...- Displacement Sensor
- High accuracy
- High brightness
- Broad bandwidth
- Thickness measurement
-
The replacement of human work with AI has been promoted in recent years because the labor shortage in the manufacturing industry has become remarkable 1). In particular, anomaly detection by AI image inspection has come to be used. On the other hand, image inspection cannot detect abnormalities, such as insufficient axial force, in screw tightening due to the lack of difference in appearance. In this paper, we propose a method to ...
- AI Technology
- Real-time anomaly detection
- Screw tightening
- Automation
- PLC
-
Applying the optimization methods to design for products as optimization problems is increasingly spreading. Since these methods can make design processes more efficient, we should also use them when designing power electronic converters. Design processes for power electronics converters are roughly classified into electrical circuit parameters, geometric properties of parts, and alignment ...
- Power Electronics
- Optimization method
- Design Process
- Machine Learning
- CAE
-
In recent years, there has been an increasing need for production to improve by utilizing information processing technology by utilizing the data generated by control equipment at production sites. Since the needs are diversifying and the improvement of information processing technology does not stop, there are a need for an environment where applications can quickly respond to the needs of the field ...
- IoT Technology
- Application Platform
- Application Framework
- PLC
-
In recent years, high efficiency and maintenance-free systems have been promoted in renewable energies, such as photovoltaic power generation, which are increasingly used as countermeasures against environmental problems. The increase in voltage of the system is accelerating to improve efficiency, and in order to suppress various problems in heat generation when energized with a large current, the relay used for the grid linkage ...
- Low contact resistance
- High capacity switching
- Concentrated resistance
- Switching mechanism
- Impact force
-
In the manufacturing industry, automation of manufacturing, especially the introduction of robots, is being actively promoted because of labor shortages and rising labor costs, but installation space, start-up person-hours, and flexibility at work are issues to be addressed. In particular, a 3D sensor is essential to estimating the position and orientation of parts accurately in bin picking applications, and a robot hand-mounted 3D ...
- 3D sensor
- Robot picking
- For robot arms
- Small and light
- With robustness
-
Renewable energy is an important low-carbon energy source that can contribute to energy security. A surplus electricity purchase system was started in 2009 to promote the spread of renewable energy. Since then, the purchase price has fallen, while the electricity price has risen. Therefore, the power storage system is attracting attention from the viewpoint of self-consumption in which photovoltaic power generation electricity ...
- Power storage system
- Smaller size and lighter weight
- High efficiency
- SiC-MOSFET
- Inverter switching method
-
In the product assembly process, there is the work of supplying parts randomly stacked in a container to an automated machine. This is called bin picking. In response to the recent shortage of labor at manufacturing sites and the increase in labor costs, automation of this work is required. By realizing bin picking using 3D sensors and industrial robots, it is possible to manufacture a wide variety of products using the same system, and it is possible to reduce the cost and time of the start-up of the production line. At this time, in order to realize the same speed as a human, it is important ...
- Bin picking
- 3D recognition
- Alignment
- 3D sensor
- Robotics
-
The Inspection System Division has traditionally performed 3D measurement of printed mounting boards and inspected them according to quantified quality standards. AOI (Automated Optical Inspection) and AXI (3D-CT method) inspect the shape of solder. The automated x-ray inspection, Q-upNavi, analyzes...
- Data analysis platform
- SMT
- Solder inspection
- Data warehouse
- Data mart
-
With the rising demand for body temperature measurement and recording under the COVID-19 pandemic, there had not been a variety of choices for smartphone-connected thermometers. To respond to the significant leap of needs for body temperature recording, we faced the urgent task of developing a connected thermometer ...
- Sonic Wave Communication
- Thermometer
- COVID-19
- Cross Platform
- Demodulation Algorithm
-
The wetting inspection of solder on components is the most important part of the board appearance inspection. However, solder forms various shapes because of the shape of electrodes, pads, and land. In addition, it is difficult to correctly measure the solder shape due to phenomena, such as shadows, and secondary reflections...
- Multi-CH Lighting
- Visual Inspection
- Programming Automation
- Optimization
- 3D Recognition
-
In recent years, the cost of labor for high-quality workers has been rising in Japan and other countries that have shifted from manufacturing to services, and there is a growing need to automate robots in medium- to low-volume production site, which has been done mainly by hand. Therefore, we focused on the kitting process, which is essential in the pre-assembly process of medium- and low-volume production, and examined the feasibility of ...
- Robot
- Automation
- Visual Feedback
- Tactile Feedback
- Manipulation
-
Research and development on cooperative vehicle infrastructure systems are being promoted for realizing a safe and smooth transportation society. Information from sensors installed in the road infrastructure is used for this system. Millimeter-wave radar is attracting much attention as a next-generation infrastructure sensor that is less affected by the weather, such as...
- Millimeter-wave Radar
- 3D Imaging
- Infrastructure Sensor
- Driving Safety Support Systems
- Doppler Radar
-
2022/06/13
Consideration of Improving Machining Accuracy by Disturbance Correction Using Machine Learning
At the manufacturing site, it is necessary to improve processing accuracy while maintaining and improving productivity. As a result, in recent years, variations and fluctuations in materials and machines at manufacturing sites cannot be ignored. At the manufacturing site, in order to suppress such disturbance effects, various control...- AI technology
- PLC
- Feedforward control
- Disturbance correction
- Servo press machine
-
In the casino industry, which is a tourism industry that provides entertainment and leisure time creation and amusement for people, the direction for attracting players to casino machines has been evolving rapidly in recent years, and the visual area has been expanding year by year. However, the SPIN button, which is an important button for starting a game,...
- Mechanical components development
- Thin structure
- Transparent structure
- High durability
- Impact resistance
-
We report on the development of a highly reliable safety system that ensures that the equipment continues to operate while maintaining safety functions without making emergency stops due to system errors caused by soft errors. As semiconductor devices become more highly integrated and miniaturized, transient bit errors (soft errors) in memory are a problem....
- Soft error
- Functional safety
- Reliability
- Safety PLC
- Data recovery
-
In order to enable persons and robots to work in the same shared space at manufacturing sites, robot trajectory planning technologies have been developed for robots to avoid collisions with persons during operation. However, by conventional technologies, since the operation must be temporarily stopped before the robot performs collision avoidance,...
- Machine learning
- Human trajectory prediction
- Interactive manufacturing system
- Collaborative robot
- Trajectory planning for robot manipulator
-
The Great Hanshin-Awaji Earthquake of 1995 and the Great East Japan Earthquake of 2011 resulted in a large-scale disaster, such as building collapses and fires. Therefore, it is recognized that the grasp of building damage is important for the early reconstruction of the region and...
- Verification Technology
- Earthquake
- Simulation
- Acceleration
- Vibration Sensors
-
Recently, high-speed switching circuits using GaN GIT have attracted attention for higher power density. In particular, GaN GIT devices have an ultrafast speed capability but tend to cause false turn-ons due to a lower threshold voltage. A simple RC-type gate drive method is usually used to prevent the false turn-on phenomenon....
- Power Electronics
- Wide Gap Semiconductor
- Gate Drive Circuit
- Spike gate voltage
- High Frequency
-
2021/12/13
Derivation of Arc Length Calculation for DC High Voltage Arc Interruption in Closed Space
In recent years, the higher efficiency of systems has been promoted in renewable energy represented by photovoltaic power generation, which is increasingly used as a countermeasure against environmental problems. These systems consist of high voltage DC systems....- High capacity of relay
- Arc control
- Arc discharge phenomenon
- Arc interruption performance improvement
- Environmental energy management equipment
-
Magnetic materials like ferrite, which is used in power supply circuits that handle high currents, such as DC/DC converters, exhibit a rapid decrease in inductance due to the influence of the magnetic flux generated as the DC current component increases. This phenomenon is called DC superposition,...
- DC Superposition
- Minor Loop
- Magnetic field analysis
- Incremental Permeability
- Power Electronics
-
In the manufacturing industry, it is important to identify the optimal production conditions using statistical methods, such as design of experiments. However, the number of experiments is often reduced through the use of knowledge and other means, which leads to lack of accuracy in the response surface model (RSM) for predicting product quality....
- Transfer learning
- Design of experiments
- Support vector regression
- Quality control
- Optimal production conditions
-
In recent years, 3D TOF sensors that can acquire three-dimensional information with a wide viewing angle have attracted attention for the various service robots, such as autonomous driving robots used in factories and nursing care robots. Since 3D TOF sensors can acquire spatial information, they are expected...
- Distance sensor
- TOF (Time of Flight)
- 3 dimensions
- High accuracy
- Distance image
-
Rapidly changing market needs have resulted in the demand for shorter launching times for production facilities. In conventional methods where only physical machines were used, production facility launches took longer because of stand-by time and teaching positions and orientations of robots. A virtual launching...
- Virtualization
- Integrated development environment
- Simulation
- PLC
- Robot
-
In recent years, due to soaring labor costs and the spread of a new type of coronavirus, there has been an increasing demand to save labor at the production sites. However, the need for industrial robots, especially vertical articulated robots, has been increasing as one of the laborsaving measures,...
- Robot
- Path Planning
- Trajectory Planning
- Trajectory Optimization
- Collision Checking
-
In an imaging system with multi-CH lighting, this paper addresses the issue of optimizing the lighting conditions and the imaging conditions of the camera so that they are suitable for visual inspections. The proposed method establishes a technique for accurately simulating an image of a workpiece...
- Lighting Optimization
- Visual Inspection
- Multiobjective Optimization
- Lighting Simulation
- Multi-CH Lighting
-
We are developing a ping-pong robot called FORPHEUS that can keep a table tennis rally going and interact with people to generate an appeal for harmonization, which is the future relationship between humans and machines. Although the performance of the table tennis robot has been improving year by year,...
- Ping Pong Robot
- Motion Analysis
- Vital Sensing
- Emotion Estimation
- Meta AI
-
Traditionally, system behaviors has been expressed by creating activity and sequence diagrams in the system design of the PCB Inspection System. However, it is difficult to specify the abnormal behaviors of the systems in the design phase to prevent the inclusion of defects as the system becomes highly functional...
- STAMP
- STPA
- Factory Automation
- Software Engineering
- Hazard Analysis
-
Various interactive manufacturing systems are developing to enable humans and robots to produce products in cooperation. For safety designers who design the safety of interactive manufacturing systems face difficulties to select a practical safety design method. The origin of this issue is a lack of appropriate safety standards...
- Interactive
- Interactive manufacturing system
- Machinery safety
- Risk assessment
- Safety
-
By the arrival of the IoT era, embedded devices that connect to the Internet are being exposed to cyberattacks1). In order to provide products that users can use with assurance, it is necessary to analyze security threats and take countermeasures to avoid important cyberattacks. OMRON....
- IoT
- Security
- Threat analysis
- Secure by design
- Software engineering
-
As a variety of social issues have been noticed in recent years, various programs and projects are now conducted to resolve the issues. In many cases however, whether these programs and projects have been effective is actually not evaluated. Under this circumstance, Social Impact Measurement is....
- Social impact measurement
- Logic model
- Outcome
- Health behavior
- Social issues
-
The environment for constructing information systems, such as faster networks, lower costs, and larger storage capacity, is becoming available at the production site. With these technologies, OMRON realizes an information system that covers the sensor level using the open network IO-Link as a future factory. And the....
- Information driven system
- Safety light curtain
- IO-Link
-
Recently, because of the growing need for automation of monitoring, machine learning has become widely used in the social systems domain. However, the issue of machine learning is that the pre-trainedmodel provides poor performance when the environment changes. Especially in the social systems domain, there are various....
- Artificial Intelligence
- Machine Learning
- Image Recognition
- Transfer Learning
- Optimization
-
2020/11/12
Solder Vibration Printing Technology that Enables Mixed Mounting from 0402 to Large Components
The size of passive components mounted on boards composing a product has been decreasing. Mainstream size will be 0603 (0.6 × 0.3 mm) and 0402 (0.4 × 0.2 mm), whereas the conventional sizes are 1608 (1.6 × 0.8 mm), 1005 (1.0....- Surface mount
- Solder paste printing
- 0402M
- Ultrasonic vibration
- High aspect ratio
-
OMRON HEALTHCARE Co., Ltd., is working on the development of a watch-type wearable blood pressure monitor that makes it possible to measure blood pressure anytime, anywhere. The increase in measurement opportunities from the realization....
- Blood pressure monitor
- Arterial compression technology
- Cuff
- Oscillometric methods
- Pulse sensing
-
2020/11/12
Innovation of the Method for Balancing Trade-off Requirements in the Product Design Process
One of the common subjects among the product development is the excess of development lead-time and cost, and the degradation of the products due to the redesign work by the problems that occurred at later parts of the product development....- Design Optimization
- CAE application technology
- Trade-off balancing
- Design quality improvement
- Design knowledge formalization
-
There is a growing need for miniaturization and high capacity of electronic components along with the trend of miniaturization and energy saving of the equipment, but these requirements have increased the influence of heat on electronic....
- Thermal deformation
- Resin parts
- Anisotropic material
- CAE
- Molding material
-
With the spread of IoT, embedded devices are also connected to the Internet, which is in danger of security attacks. If a security attack stopped the control of embedded devices, substantial damage is expected. Therefore, a measure is demanded....
- Cybersecurity
- Embedded device
- Attack detection
- Attack classification
-
In this paper, we deal with the grasping points estimation for robotic bin picking. Usually, grasping points are estimated by using 3D CAD of the object to be grasped. However, it becomes difficult to estimate the grasping points for non-rigid objects....
- Bin picking
- Grasping point estimation
- Robotics
- 3D recognition
- Depth map processing
-
In recent years, because of growing concerns about environmental issues, the bonding of dissimilar materials (metal and resin, etc.) has been increasing for the purpose of improving the energy efficiency of products by miniaturization and weight reduction....
- Adhesive
- Thermal cure
- Spot heat
- High-speed curing
-
The demand for oxygen concentrators that support COPD (chronic obstructive pulmonary disease) patients will increase in the future. The device supplies oxygen generated by concentrating the surrounding air, and it is necessary to monitor the oxygen....
- Thermal Gas Sensor
- Oxygen Concentration Measurement
- Trinary Gas
- MEMS
- Oxygen Concentrator
-
In the visual inspection of the substrate, the crystal structure becomes irregular when the electrode is in the form of a thin film, causing an inconsistent color in the reflection characteristics when imaging is performed using coaxial lighting. The inconsistent....
- Lighting
- Lighting conditions
- Visual inspection
- Phased search
- MDMC
-
We propose a novel method for on-site software customization to improve performance of facial image sensing. In cases that a user has the following facial characteristics, it is difficult to perform facial image sensing with high accuracy....
- Facial Image Sensing
- On-site Customization
- Machine Learning Algorithm
- Data Collection System
- Driver Monitoring
-
2020/11/12
Millimeter-Wave Traffic Monitoring Radar using High-Resolution Direction of Arrival Estimation
Driving safety support and automated driving technology have attracted much attention for realization of a safe transportation society. Infrastructure coordinate system is expected to play an....- Millimeter-wave Radar
- Automated Drive
- Driving Safety Support Systems
- Antenna Control
- Direction of Arrival Estimation
-
2020/11/12
Development of Temperature Prediction Technology for Early Detection of Panel Abnormalities
In recent years, power outages and ignition accidents caused by abnormal temperature rises in panel components due to aging of facilities have been increasing. Consequently, for example....- Machine Maintenance
- Predictive maintenance
- Thermal monitoring
-
There are two problems that arise of generating more wiring work for sensors with a tooling change in high-mix low-volume production and increasing downtime by breaking. Therefore, the introduction of a wireless interface is considered. There....
- Directivity control
- Microwave power transfer
- RFID
- Wireless sensor
- Multipath fading
-
In recent years, it has been necessary to improve operational efficiency and reduce costs by using AI and IoT in the manufacturing industry to reduce the impacts from the shortage of skilled workers and increased labor costs. To meet these requirements, the amount....
- Switched Mode Power Supply
- Noise Cancelling
- Miniaturization
- Power factor correction
-
In recent years, the growing interest in environmental problems has stimulated the urgent spread and efficiency improvement of renewable energy. Energy efficiency increases the rated voltage and the current of electrical devices, and the devices require higher interruption....
- High electrical durability relay
- Simulation technology to quantify arc interruption phenomena
- Analysis for electromagnetic and thermal phenomena
- Energy management device for environmental usage
- Improvement for arc interruption
-
2020/11/12
Development of Small Size, Lightweight, High Efficiency Outdoor Single Phase Solar Inverter
Photovoltaics is attracting attention because it reduces the global environmental load and improves the energy self-sufficiency rate. However, the power generation cost of photovoltaics in Japan is about 1.6 times higher than that of the....- Solar inverter
- Downsizing and weight reduction
- High efficiency
- Two phase interleaved boost chopper
-
In recent years, “IoT (Internet of Things)”, in which all “things” are connected by a network, has attracted attention. In IoT, advanced sensing devices that can process and transmit sensing data are being expected in order to create new services...
- IoT
- Environmental sensor
- Wireless
- USB Power supply
- Algorithm
-
2020/03/10
Application of monitoring technology for social infrastructure (2)
Proposal of evaluation method of deterioration/damage and result of field experiment under SIP projectInfrastructure built in the period of high economic growth in Japan is becoming deteriorated. However, there are some social issues to maintain and manage. In addition to an increase in the number of structures that need...- infrastructure
- bridge
- maintenance
- monitoring
- structural analysis
-
2020/03/10
Application of monitoring technology for social infrastructure (1)
For validation and achievement of monitoring system with high site applicabilityIn 2022, over 40% of bridges with a bridge length of 2 m or more have reached an aging era exceeding 50 years after completion of bridges in Japan. In addition, engineers of the baby-boomer generation retire and the technical shortage to maintain...- monitoring
- Power-saving, low power
- wireless
- acceleration
- strain
-
Many companies have call centers to answer telephone calls from their customers. Call centers’ two major indices, service quality and running costs, have a trade-off relation; improving service quality needs additional operators, who require additional costs...
- AI
- Time Series Analysis
- Space State Model
- Prediction
- Call Center
-
Recently, manufacturers have some common issues such as highly developed manufacturing, complicated manufacturing, or manufacturing with few skilled people. They are trying to solve these issues by IoT technologies based on big-data which are...
- Auto Web Inspection System
- Quality Control
- BI
- Condition Based maintenance
- Internet of Things
-
2020/03/10
Simulation technology to predict dynamic motion of relay
Simulation technology for realizing high capacity of relayIt is very important for design to predict the dynamic motion of contact for realizing downsizing and high capacity for a mechanical relay along with trend of downsizing of application devices and saving energy. In order to predict the dynamic motion of contact...- Coupled analysis
- Dynamic motion analysis
- Contact bounce
- Breaking velocity
- High capacity of relay
-
In the manufacturing industry, there is lack of engineers who are responsible for maintenance, due to environmental changes such as a declining birth rate and an aging population. In addition, the existing equipment has becoming decrepit, so the frequency...
- Temperature Controller
- Equipment Maintenance
- Anomaly Detection
- System Identification
- Condition Based Maintenance
-
Not only high-function electronic products such as PCs and smartphones but also the products such as FA equipment and power electronics products have being downsized. The heat capacity of the printed wiring board (PWB) is increasing due to multi-layering...
- JISSO technology
- Wave soldering
- Process control
-
Many electronic devices such as relays, switches and FA sensors are used in the various environments, and they are protected by seal to guarantee their movements. In particular, in applications where outdoor use, water including salt (saltwater) such...
- Seal
- Saltwater intrusion
- Penetration distance estimation
- Evaluation technology
- Electronic equipment
-
In the board mounting industry, there are an increasing number of parts and boards that are difficult to be insepected with AOI because solder is invisible. And high quality requirements such as bonding strength of the automobile industry and full surface...
- CT
- X-ray
- Automatic inspection system
- Inline
- Solder inspection
-
2020/03/10
The Ping Pong Robot to Return a Ball Precisely
~ Trajectory Prediction and Racket Control for Spinning Balls ~We are developing a ping-pong robot “FORPHEUS” that can play table tennis with humans representing the harmony between humans and machines. In order to accurately return the ping-pong ball, the robot must perform the following tasks: predicting the trajectory...- Robotics
- AI
- Optimization
- Kinetic analysis
-
The size of passive components mounted on the boards composing the product has been increased from the conventional 1608M (1.6 × 0.8 mm) and 1005M (1.0 × 0.5 mm) to 0603M (0.6 × 0.3 mm) and 0402M (0.4 × 0.2 mm) are becoming mainstream. Though these parts...
- JISSO Technology
- Solder printing
- Solder paste
-
In recent years, it has become important to make a full use of sensing data from control devices like sensors via new IT technology such as AI. To accelerate this, it is important to collect and transform ill-formed sensing data from control devices to...
- IoT
- PLC
- Data formatting
- Control device specification
- Automatic generation of programs
-
With increasing high-mix low volume production in manufacturing industry, more flexible production facility is required for rearrangement of factory layout. Wireless pushbutton switch requires no signal line and no power supply line by internal...
- Wireless pushbutton switch
- Wireless communication
- Communication reliability
- Notification indicator
- Energy Harvesting
-
Software is becoming larger and more complex mainly due to higher functionality of the product, software implementation of functions what used to be realized by hardware. As a result, increasing development and quality costs, frequent schedule...
- Software Engineering
- Software Product Lines
- Software Architecture
- Human Resource Development
- Process Improvement
-
2020/03/10
Development of AI-equipped Machine Automation Controller (2)
Data collection synchronized with machine control and realization of Time-Series databaseIn recent years, in the manufacturing industry, the need to utilize AI (Artificial Intelligence) and IoT (Internet of Things) at the manufacturing site continues to rise in order to improve availability of facilities and stably produce high quality...- Time-series Database
- Embedded Database
- AI Technology
- NoSQL
- Edge Computing
-
2020/03/10
Development of AI-equipped Machine Automation Controller (1)
Implementation of AI system usable by maintenance personnel and installation of AI function in machine automation controllerAt the manufacturing site, the labor force is chronically short. In the future, productivity is expected to decline due to a decrease in skilled technicians, and there is a demand for labor saving. In view of these backgrounds, we are promoting labor saving by...- AI
- Real-time anomaly detection
- Equipment maintenance
- PLC
- Predictive maintenance
-
Along with the recent global trend, consumer needs in the market are getting more diversified, and manufacturers are required to produce new products in a short cycle. Manufacturing companies have installed new equipment and added new production...
- PLC
- Open Source
- Git
- Concurrent development
- Integrated factory automation development environment
-
2020/03/10
Development of AI-Equipped Machine Automation Controller (3)
Generation of anomaly detection models at manufacturing siteIn recent years, the need has continually risen for the introduction of AI and the internet of things (IoT) on manufacturing floors. It allows manufacturers to contain the impact of skilled worker shortages and surging labor costs, while...- Artificial intelligence technology
- Real time anomaly detection
- Equipment maintenance
- Programmable Logic Controller
- Machine learning algorithm
-
2020/03/10
Stable reading for UHF RFID
Technique for preventing erroneous detection of non-target RF tagIn the automotive industry, the increase in the number of recalls is a problem. In order to respond quickly when a recall occurs, there is likewise an increasing importance of individual part identification to identify when and where all...- RFID
- Stable communication
- Post-installation adjustment
- Traceability
- RF tag
-
In recent years, manufacturing companies need to respond the request of “multi-variety, variable-volume production” in the era of diversified needs. Along with that, they also need to develop safety systems that can be flexibly modified...
- Automation Software Sysmac Studio
- Safety Controller
- Programming expertise
- Reduction of safety system design man-hours
- PLCopen Safety
-
In production lines, stable operation of machines is one of the most important factors so that it is required to have scheduled maintenance at the right timing. In most maintenance scenes, maintenance personnel will...
- Three-phase motor
- Maintenance
- Insulation resistance
- Minute leakage current
- Leakage current of inverter-driven motor
-
In recent years, the importance of traceability is increasing to respond to quality problems such as recall of automobile industry. In order to realize traceability and fulfill its social responsibility, companies...
- Image Processing
- Automatic recognition technology
- Two-dimensional symbols
- Data Matrix
- DPM(Direct Part Mark)
-
In this paper, we propose a technique to detect various defects in uniform background objects (hairline, satin, etc.) in visual inspection system. “Human resources shortage” and “ diversification of consumer needs...
- AI
- Deep Learning
- Visual Inspection
- CPU Optimization
-
2020/03/10
The progress in displacement sensor technology by the change of application scene in manufacturing
High Accuracy / High Speed for Realizing Stable Measurement during ScanningConventional triangulation method has been the mainstream for displacement sensors, but on leading-edge manufacturing of customers, there have been the problems of the tuning difficulties when setting by the...- Displacement sensor
- High precision
- High speed
- Optical design
- Algorithm
-
Recently, manufacturers of printed circuit boards are required more high quality and more cost competitiveness. Therefore the manufacturing lines must keep high quality autonomously without human skills and work.Omron...
- Real-time anomaly detection
- Potential defect prevention
- Quality management
- SMT
- Solder inspection
-
2019/12/13
Development of AI Technology for Machine Automation Controller (1)
Anomaly Detection Method for Manufacturing Equipment by Utilizing Machine DataThe equipment maintenance and production management for manufacturing, which have been dependent on experience and knowledge of workers, are being improved by AI, IoT, and big data. It is necessary to collect and analyze...- AI Technology
- Real-time anomaly detection
- Equipment maintenance
- Programmable logic controller
- Machine learning algorithm
-
2019/12/13
Development of AI Technology for Machine Automation Controller (2)
The Insight Gained Through Implementation of Anomaly Detection AIs to the Machine Controller.Recently, activities of productivity improvement have been attempted at production sites with predictive approaches. Cloud-based machine monitoring systems were once introduced but were not prevailing due to cost...- AI machine automation controller
- Anomaly detection AI
- High speed and light
- Monitoring and analyzing
- Isolation forest
-
2019/12/13
ILO integrated control technology
Control technology contributing to innovation in manufacturingTo solve various control problems in the manufacturing process, Omron pursues advanced integrated control technology of ILO(Input-Logic-Output). In addition to providing ILO devices capable of high-speed and highprecision...- ILO integrated control technology
- Machine automation controller
- Model predictive control
- Visual feedback control
- Control theory
-
2019/12/13
Sensor Technology to Realize Continuous Blood Pressure Monitoring
Development and Practical Application of High-precision Multi-element MEMS Pressure SensorOMRON HEALTHCARE Co.,Ltd. is developing new technology to enable beat-by-beat blood pressure monitoring. The conventional oscillometric equipment was unable to measure blood pressure continuously and...- Continuous blood pressure monitoring
- Non-invasive blood pressure monitoring
- Tonometry method
- MEMS pressure sensor
- Stress simulation
-
2019/12/13
Driver Status Monitoring System in Autonomous Driving Era
Driver Status Estimation with Time-series Deep LearningWe propose a novel driver’s status estimation system based on driver’s behavior in autonomous driving scene. In future years, drivers are expected to be responsible for driving and monitoring the surrounding environment...- Autonomous driving
- Driver status monitoring system
- Time series deep learning
- Technology for sensing driver’s concentration level
- Near infrared camera
-
2019/12/13
Development of the in-vehicle pulse sensor
About the pulse rate estimate technique from a microwave sensorIn late years accidents due to the health condition of the driver are increasing. The precaution is required all the more.Therefore we developed the in-vehicle pulse sensor using the microwave sensor. We installed...- In-vehicle pulse sensor
- Pulse rate estimate algorithm
- Pulsation period signal detection
- Microwave doppler sensor
- Synchronous detection
-
2019/12/13
Parking Sensor based on geomagnetic variations of vehicle
Algorithm based on unique geomagnetic variationsIn this paper, we discuss about vehicle detection technique for the Parking Sensor. Previous technique like electromagnetic induction loop coil, Ultrasonic sensor and Image processing has a problem such as restriction on installation...- Wireless geomagnetic vehicle sensor
- Parked vehicle detection algorithm
- Autonomous driving
- Geomagnetism detection element
- Engine section detection algorithm
-
In order to reduce the volume and cost of the PCS (Power Conditioning System), miniaturization of AC reactors (ACL) of inverters has been studied. If the ACL impedance value becomes smaller than the Grid-impedance...
- Power conditioning system
- Miniaturization of AC reactor
- Grid impedance estimation method
- Impedance suppression compensator
-
2019/12/13
Development of a new system using extraordinarily small self-controlled run robot
About a challenge to automation in small-lot productionIn recent years, in order to grow further while maintaining its competitiveness in the environment surrounding the electronic parts business(Electronic &Mechanical Components, hereinafter referred to EMC)...- Extraordinarily small self-controlled run robot
- New production system
- Functional investment analysis
- Low-cost pickup and placing robot
- Nonsynchronous transfer
-
2019/12/13
Dynamics simulation technology for high electrical durability relay
Electrical durability design by numerical analysis approachRecently energy efficiency improvement of electrical equipment is promoted as environmental issues. This trend also accelerates both downsizing and switching capability for mechanical relays. We need to control...- High electrical durability relay
- Dynamics simulation technology
- Electrical durability design
- Electromagnetic analysis
- Eco-friendly equipment
-
2019/12/13
Development of air quality sensor for air purifier
Accuracy enhancement by optical system and dust collection structureAir pollution by fine particulate matter PM 2.5 is becoming a big topic and increasing people’s interest. PM2.5 sensors are installed in air purifiers in our immediate surroundings vicinity and are also pervasive...- Air purifier
- Microparticle detection sensor
- High-sensitive photo IC
- Dust collection structure
- High frequency wave filtering
-
2019/12/13
Study and development of low-noise MEMS acoustic sensors
Important considerations for air damping and process stabilityAcoustic sensing technology like speech recognition or noise cancellation has attracted a lot of attention recently. These new applications stimulate the demand for smaller and lower noise MEMS (micro electro-mechanical system)...- MEMS acoustic sensor
- Slit diaphragm structure
- Reduction of self-noise
- Layout of narrow-pitch openings
- Etching process stabilization technology