OMRON TECHNICS -Technical Papers-
This webpage introduces technical papers that describe the outcomes of the OMRON Group’s R&D activities, as well as the technologies that support its products and services.
-
Today, in-factory logistics faces the social challenge of labor shortages while the importance of parts management increases. To address this, automation aimed at reducing human labor is being implemented, and there is a demand for advanced material and parts management system functions on-site. ...
- UHF RFID
- Estimation Algorithm
- Traceability
- Luggage Management
- Automation
-
In recent years, deep learning algorithms have been applied to sensing and are contributing to the enhancement of high-precision devices, such as image sensors. This study aims to apply deep learning algorithms to simple sensors that handle one-dimensional signals with the goal of improving accuracy ...
- Embedded device
- AI Technology
-
2025/08/25
Development of Middleware for Rapid Prototyping of Robots Based on Parallel Behavior Architecture
To realize robots that can move flexibly in human environments and automate nonstandard tasks, it is essential to parallel process functions like recognition, planning, and control to enhance responsiveness. The parallel behavior architecture addresses this requirement by executing high-level ...- Robot Middleware
- Robot System
- Real-time Control
- Parallel Processing
- Rapid Prototyping
-
In various fields, including medical and health management, the demand for vital sensing technology is increasing because of the proliferation of related services. One of them, millimeter-wave radar, is seen as a promising technology that can simultaneously measure the vital signs of multiple people in a noncontact manner with the body. ...
- Radar
- Vital measurement
- Clustering
- Respiratory rate
- Time series
-
2024/12/10
Reduction of Waveform Discontinuity in Respiratory Waveform Measurement using Millimeter-Wave Radar
Human sensing, which measures human movements and vital signs, has become familiar to us with the proliferation of measurement devices and the expansion of related services. Among the various measurement devices, millimeter-wave radar has attracted much attention because it can accurately measure human ...- Millimeter-Wave Radar
- Vital Sensing
- Respiratory Waveform
- Discontinuity
- Waveform Analysis
-
Millimeter-wave radars have been drawing interest as a means of contactless sensing of the positions of people and objects and are expected to be used in a wide range of fields, such as automotive, transportation infrastructure, factory automation (FA), and healthcare. In order for radars to correctly detect the position of the targets, it is necessary to estimate the direction of arrival of the radio waves with high accuracy. ...
- Millimeter-wave Radar
- Estimating Direction-of-arrival
- Waveguide
- SIW
- Suppressing Unnecessary Radiation
-
We are developing a ping-pong robot called FORPHEUS that can keep a table tennis rally going and interact with people to generate an appeal for harmonization, which is the future relationship between humans and machines. Although the performance of the table tennis robot has been improving year by year,...
- Ping Pong Robot
- Motion Analysis
- Vital Sensing
- Emotion Estimation
- Meta AI
-
With the spread of IoT, embedded devices are also connected to the Internet, which is in danger of security attacks. If a security attack stopped the control of embedded devices, substantial damage is expected. Therefore, a measure is demanded....
- Cybersecurity
- Embedded device
- Attack detection
- Attack classification
-
The demand for oxygen concentrators that support COPD (chronic obstructive pulmonary disease) patients will increase in the future. The device supplies oxygen generated by concentrating the surrounding air, and it is necessary to monitor the oxygen....
- Thermal Gas Sensor
- Oxygen Concentration Measurement
- Trinary Gas
- MEMS
- Oxygen Concentrator
-
In recent years, “IoT (Internet of Things)”, in which all “things” are connected by a network, has attracted attention. In IoT, advanced sensing devices that can process and transmit sensing data are being expected in order to create new services...
- IoT
- Environmental sensor
- Visual Inspection
- Wireless
- Algorithm
-
2020/03/10
The Ping Pong Robot to Return a Ball Precisely
~ Trajectory Prediction and Racket Control for Spinning Balls ~We are developing a ping-pong robot “FORPHEUS” that can play table tennis with humans representing the harmony between humans and machines. In order to accurately return the ping-pong ball, the robot must perform the following tasks: predicting the trajectory...- Robotics
- AI
- Optimization
- Kinetic analysis
-
2019/12/13
Study and development of low-noise MEMS acoustic sensors
Important considerations for air damping and process stabilityAcoustic sensing technology like speech recognition or noise cancellation has attracted a lot of attention recently. These new applications stimulate the demand for smaller and lower noise MEMS (micro electro-mechanical system)...- MEMS acoustic sensor
- Slit diaphragm structure
- Reduction of self-noise
- Layout of narrow-pitch openings
- Etching process stabilization technology