OMRON

Corporate | Global
PRINT
  • Application of monitoring technology for social infrastructure (2)

    Proposal of evaluation method of deterioration/damage and result of field experiment under SIP project
    Infrastructure built in the period of high economic growth in Japan is becoming deteriorated. However, there are some social issues to maintain and manage. In addition to an increase in the number of structures that need...
    Nishida Hideshi / Takase Kazuo / Hatayama Goro / Sasaki Eiichi
    • infrastructure
    • bridge
    • maintenance
    • monitoring
    • structural analysis
  • Application of monitoring technology for social infrastructure (1)

    For validation and achievement of monitoring system with high site applicability
    In 2022, over 40% of bridges with a bridge length of 2 m or more have reached an aging era exceeding 50 years after completion of bridges in Japan. In addition, engineers of the baby-boomer generation retire and the technical shortage to maintain...
    Kuroda Takuya / Nishida Hideshi / Ozaki Tomohiro / Hinoue Tomohiko / Akai Ryota
    • monitoring
    • Power-saving, low power
    • wireless
    • acceleration
    • strain
  • Driver Status Monitoring System in Autonomous Driving Era

    Driver Status Estimation with Time-series Deep Learning
    We propose a novel driver窶冱 status estimation system based on driver窶冱 behavior in autonomous driving scene. In future years, drivers are expected to be responsible for driving and monitoring the surrounding environment...
    Hyuga Tadashi / Kinoshita Koichi / Nishiyuki Kenta / Hasegawa Yuki
    • Autonomous driving
    • Driver status monitoring system
    • Time series deep learning
    • Technology for sensing driver窶冱 concentration level
    • Near infrared camera
  • Development of the in-vehicle pulse sensor

    About the pulse rate estimate technique from a microwave sensor
    In late years accidents due to the health condition of the driver are increasing. The precaution is required all the more.Therefore we developed the in-vehicle pulse sensor using the microwave sensor. We installed...
    Mitani Shigetomo
    • In-vehicle pulse sensor
    • Pulse rate estimate algorithm
    • Pulsation period signal detection
    • Microwave doppler sensor
    • Synchronous detection
  • Parking Sensor based on geomagnetic variations of vehicle

    Algorithm based on unique geomagnetic variations
    In this paper, we discuss about vehicle detection technique for the Parking Sensor. Previous technique like electromagnetic induction loop coil, Ultrasonic sensor and Image processing has a problem such as restriction on installation...
    Yoshino Kotaro / Watanabe Makoto / Kanda Shohei
    • Wireless geomagnetic vehicle sensor
    • Parked vehicle detection algorithm
    • Autonomous driving
    • Geomagnetism detection element
    • Engine section detection algorithm
Page
Top