OMRON Releases New Programmable Terminal NA Series Using ICT - Boosting Productivity and Minimizing Downtime -
November 4, 2014
Kyoto, Japan -- OMRON Corporation (TSE: 6645, ADR: OMRNY) today announced the November release of its new NA series programmable terminal which helps improve capacity utilization of machines by displaying multimedia and sharing information via mobile devices.

The NA-series programmable terminal is the interface between operator and machine in the Sysmac automation platform (*1).
To improve productivity by increasing capacity utilization, all workers are required to share data on each device incorporated in machines in real time and solve various problems quickly. The NA series provides the system to display real-time device data on remote tablets and PCs through Ethernet or Wi-Fi in addition to on its own screen. This allows both machine operators and authorized people inside and outside the factory to access the same information instantly. Fast troubleshooting and improvement will increase productivity.

Powerful graphics and multimedia function provide operators with how to perform troubleshooting procedures in an understandable way by showing documents including PDFs and playing video files (*2) in the latest format. Accurate troubleshooting will minimize machine downtime.
New Programmable Terminal NA Series Using ICT (http://www.ia.omron.com/products/family/3405/)
Features
-
One Software: Integrated development environment to cut development time
- The NA series and other devices integrated into the Sysmac automation platform can be controlled in one project.
- NJ controller variables can be shared in the NA project, which speeds up development when variables are added due to specification changes.
- Visual Basic is used for programming. This globally used programming language makes it easy to secure machine designers worldwide.

-
Keep Machine Running: Securing stable machine operation using the latest ICT
- Increased security features prevent unexpected machine stops.
- Guidance displayed in the latest document viewer and multimedia player assists troubleshooting.
- Real-time machine data can be displayed on remote tablets and PCs to share the information all over the world as well as in the factory.

-
My HMI: Simple and fast interface development with structured projects and reusable, customizable objects
- Users can design their own objects by combining other objects and Visual Basic.
- OMRON provides libraries of frequently-used objects to simplify and accelerate the development process.

Ordering Information
NA
| Product name | Specifications | Model |
|---|---|---|
| NA5-15W | 15.4 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 1280 x 800 dots, Frame color: Silver |
NA5-15W101S |
| 15.4 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 1280 x 800 dots, Frame color: Black |
NA5-15W101B | |
| NA5-12W | 12.1 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 1280 x 800 dots, Frame color: Silver |
NA5-12W101S |
| 12.1 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 1280 x 800 dots, Frame color: Black |
NA5-12W101B | |
| NA5-9W | 9 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 800 x 480 dots, Frame color: Silver |
NA5-9W001S |
| 9 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 800 x 480 dots, Frame color: Black |
NA5-9W001B | |
| NA5-7W | 7 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 800 x 480 dots, Frame color: Silver |
NA5-7W001S |
| 7 inch wide screen, TFT LCD, 16,770,000 colors (24 bit full color), 800 x 480 dots, Frame color: Black |
NA5-7W001B |
Automation Software
| Product name | Specifications | Number of licenses | Media | Model |
|---|---|---|---|---|
| Sysmac Studio Standard Edition Ver.1.[][] |
The Sysmac Studio is the software that provides an integrated environment for setting, programming, debugging and maintenance of machine automation controllers including the NJ series, EtherCAT slaves, and the HMI. Sysmac Studio runs on the following OS. OS: Windows XP (Service Pack 3 or higher, 32-bit version) / Vista (32-bit version) / 7 (32-bit/64-bit version) / 8(32-bit/64-bit version) / 8.1(32-bit/64-bit version) |
--- (Media only) |
DVD | SYSMAC-SE200D |
| 1 license | --- | SYSMAC-SE201L |
Multi licenses are available for the Sysmac Studio (3, 10, 30, or 50 licenses).
The Sysmac Studio version 1.11 or higher is required for the NA series.
About OMRON Corporation
OMRON Corporation is a global leader in the field of automation based on its core technology of sensing and control. OMRON's business fields cover a broad spectrum, ranging from industrial automation and electronic components to automotive electronic components, social infrastructure systems, healthcare, and environmental solutions. Established in 1933, OMRON has over 36,000 employees worldwide, working to provide products and services in more than 110 countries and regions.
In the field of industrial automation, OMRON supports manufacturing innovation by providing advanced automation technologies and products, as well as through extensive customer support, in order to help create a better society. For more information, visit OMRON's website at: https://www.omron.com/.
- *1. Sysmac automation platform
Complete machine control through one software and one seamless connection with a variety of I/O devices. Machine and motion programming is fully compliant with IEC 61131-3, and the dedicated software suite features functions such as programming, motion designing and network setting meaning simplified control of all connected devices and freeing users to engage in further innovation. - *2. Playing video files
The NA series is equipped with media player that can play MPEG-4, WMV, or other video files.
- Sysmac is a trademark or registered trademark of OMRON Corporation in Japan and other countries for OMRON factory automation products.
- Windows and Visual Basic is registered trademarks of Microsoft Corporation in the USA and other countries.
- EtherCATツョ is registered trademark and patented technology, licensed by Beckhoff Automation GmbH, Germany.
- Other company names and product names in this document are the trademarks or registered trademarks of their respective companies.
- The product photographs and figures that are used in this document may vary somewhat from the actual products.
- Microsoft product screen shot(s) reprinted with permission from Microsoft Corporation.
- For more press information, please contact:
- Kiyotaka Fujiwara
OMRON Corporation Industrial Automation Company
HMI Business Development Group, ID & HMI Div., Automation Systems Division HQ
Tel: +81-75-344-7020