OMRON

Corporate | Global
PRINT

OMRON Announces "OKAO Vision Face Recognition Sensor",World's First Face Recognition Technology for Mobile Phones

FOR IMMEDIATE RELEASEFebruary 28, 2005

Kyoto 窶 OMRON Corporation (TSE: 6645; US:OMRNY), a global leader in automation, sensing and control technology, has announced “OKAO Vision Face Recognition Sensor”, a world first* in face recognition technology which can be implemented in PDAs, mobile phones or other mobile devices with a camera function. The ability to recognize and verify the authenticity of the user through face recognition is meant to contribute to greater security and safety for mobile devices, and the information they contain, in the future. The technology will be on show at the “Security Show 2005”, which will be held at the Tokyo Big Site from March 2nd to March 4th, 2005. images

“Functionality in mobile phones and other mobile devices is upgrading significantly from simple phone calls and e-mails to include a variety of access, payment and planning services. As a result, mobile devices are carrying ever more personal information including address books, schedules and payment information,” said Masato Kawade, Senior Manager of the Sensing Technology Laboratory in Kyoto. “The “OKAO Vision Face Recognition Sensor”, featuring OMRON’s “Sensing & Control” core technology, has been designed to protect this information even when the mobile phone is lost or stolen.”

Camera equipped mobile units enabled with the “OKAO Vision Face Recognition Sensor” require no additional hardware. Users register their own face image to their unit with the unit’s camera. To use the unit, the user simply takes his or her own photo. The “OKAO Vision Face Recognition Sensor” will automatically detect the user and unlock the unit. The verification process takes less than a second from snapping the photograph. Further, there is no need to adjust the camera position when taking the photo. If the face is included in the photo, the sensor will detect the owner automatically.

The new sensor is made possible with OMRON’s “OKAO Vision”, a core company sensing technology, which allows the technology to transcend previous limits in memory capacity and processing ability by successfully downsizing and speeding up the algorithm. The sensor tests successfully more than 99 times in 100, and is fully Symbian, BREW, embedded Linux, and ITRON OS compatible.Data registration measures 1.5 KB per photo, while memory usage measures just ROM 450 KB and RAM 370 KB. Full processing time is approximately one second with MSM 6500.

* This “World first” stands for a face detection and face recognition technology for mobile phone applications, as of February 28th, 2005.

Features

  1. Camera equipped mobile units enabled with the “OKAO Vision Face Recognition Sensor” require no additional hardware.
  2. The verification process takes less than a second from snapping the photograph.
  3. No need to adjust the camera position when taking the photo. If the face is included in the photo, it will automatically detect the owner’s face.

Specifications and performance

  1. 99% recognition: The sensor verifies the owner 99% or more (OMRON tests).
  2. Memory usage: ROM 450 KB, RAM 370 KB
  3. Registered data size: 1.5 KB per photo
  4. Processing time: approx. one second ( with MSM 6500)
  5. Capable OS: Symbian OS, BREW, embedded Linux, ITRON

About OMRON

Headquartered in Kyoto, Japan, OMRON Corporation is a global leader in the field of automation. Established in 1933 and headed by President and CEO Hisao Sakuta, OMRON has more than 26,000 employees in over 35 countries working to provide products and services to customers in a variety of fields including industrial automation, electronic components, social systems (ticket gate machines, ticket vending machines, and traffic control), and healthcare. The company is divided into five regions and head offices are in Japan (Kyoto), Asia Pacific (Singapore), China (Shanghai), Europe (Amsterdam) and US (Chicago). For more information, visit OMRON’s website at www.omron.com

For media related enquiries, please contact:
Takayuki Nakamura
OMRON Corporation
Corporate Brand Communications Department
e-mail: takayuki_nakamura@omron.co.jp
phone: +81-3-3436-7202

Adobe Acrobat Reader is free software that lets you view and print Adobe Portable Document Format (PDF) files.

Page
Top