Enhance the facility operation rate at automobile and automobile parts factories
OMRON To Introduce Next-generation Proximity Sensors Which Enable the World's Longest-distance*1 Detection
September 28, 2017
OMRON Corporation (HQ: Shimogyo-Ku, Kyoto. CEO: Yoshihito Yamada) will introduce on October 2 , 2017, E2E-NEXT Next-generation Proximity Sensors which enable the world's longest sensing distance and "e-jig" Mounting Sleeves, for further enhancement of facility operation rate at automobile and automobile parts factories.
The newly released E2E-NEXT has nearly double*2 the sensing distance of our previous models, thus reduce the occurrence of facility stoppages due to malfunctions and failures caused by collisions with sensing objects down to one-third at automobile and automobile parts factories. Also, "e-jig" sharply reduces the time required to replace a proximity sensor after failures: from approximately ten minutes to approximately 10 seconds. The recovery time takes an average of approximately 60 minutes after facility stoppages because of a series of works: checking failure parts, dismantling equipment partially, in addition to replacing, wiring, and checking operation of sensors. With "e-jig", you can reduce this down to approximately 50 minutes.
Through the introduction of E2E-NEXT sensors which enable the world's longest sensing distance and "e-jig" which determines the installation position of a sensor in a single operation when replacing a proximity sensor, users can reduce the unexpected facility stoppages by approximately 173 hours, which is nearly10% of the unexpected stoppages per year (approximately1,600 hours).
Automobile and automobile parts factories are assumed to lose 10 to 60 million yen if facilities stop for an hour. It is a major managerial issue to reduce the frequency and time of facility stoppages. We conducted a survey at manufacturing sites of engine parts before E2E-NEXT development. The result shows that unexpected facility stoppages totaled approximately 1,600 hours, 240 hours*3 of which (15%) were caused by malfunctions and collisions between proximity sensors and sensing objects. Increasing the sensing distance of proximity sensors enables to reduce malfunctions and collisions caused by wear and vibrations due to facility's aged deterioration. It was difficult with the existing technology, however, because the changes in ambient temperature greatly affect the stability of detection.
OMRON independently developed "Thermal Distance Control" technology and "Analog Digital Hybrid IC*4" that enable temperature compensation.
OMRON used these for E2E-NEXT to minimize the effect due to temperature changes and achieved stable long sensing distance.
OMRON's new E2E-NEXT and "e-jig" will help reduce 240 hours of unexpected facility stoppages a year due to proximity sensors down to approximately 67 hours*5 at automobile and automobile parts factories. OMRON will continue to work for the innovation of manufacturing to achieve long and stable facility operation by working on various problems at manufacturing sites.
[E2E-NEXT Product pictures]

Main features
Nearly double the sensing distance of previous models

Less facility stoppage risk with longer sensing distance
[Example: avoid collisions with sensing objects by longer sensing distance]

Technology that supports long sensing distance
"Thermal Distance Control" Technology and Analog Digital Hybrid IC "PROX2"
"Thermal Distance Control" with "PROX2" writes temperature correction values externally when shipped and minimize the sensing distance changes due to temperature changes, which could not be done by the conventional analog IC. It is industry's first for 2-wire proximity sensors to use analog digital hybrid IC "PROX2".

Shorter time to replace a sensor reduces the time required to recover

* Time required to adjust the distance when installing a Sensor. Based on OMRON investigation.
*1 With DC 2-wire models as of September 28, 2017.
*2 The sensing distance of the most representative M12 models increased from 3 mm (previous models) to 7 mm (new products).
*3 The number of times of facility stoppages is approximately 240 times and it is approximately 60 minutes per facility stoppage.
*4 Industry's first for 2-wire proximity sensors.
*5 The number of times of facility stoppages is approximately 80 times and it is approximately 50 minutes per facility stoppage.
About OMRON Corporation
OMRON Corporation is a global leader in the field of automation based on its core technology of "Sensing & Control + Think." Established in 1933, OMRON has about 36,000 employees worldwide, working to provide products and services in 117 countries. The company's business fields cover a broad spectrum, ranging from industrial automation and electronic components to automotive electronics, social infrastructure systems, healthcare, and environmental solutions. In the field of industrial automation, OMRON supports manufacturing innovation by providing advanced automation technology and products, as well as through extensive customer support, in order to help create a better society. For more information, visit OMRON's website: https://www.omron.com/
- Contact (media):
- Corporate Communications Department
OMRON Corporation
Tel: +81-75-344-7175 - Contact (product information):
- Sensor Division,
Product Business Division HQ,
Industrial Automation Company,
OMRON Corporation
TEL: +81-75-344-7022