OMRON

OMRON SINIC X Corporation | Global

Masashi Hamaya

2025/10/09

OMRON SINIC X to Present Latest Research Findings at IROS 2025, Top-Tier Conference on Robotics

OMRON SINIC X Corporation (HQ: Bunkyo-ku, Tokyo; President and CEO: Masaki Suwa; hereinafter “OSX”) will present the latest research findings at the 2025 IEEE/RSJ International Conference on Intelligent Robots and Systems (IROS 2025). Along with ICRA1), IROS is one of the largest and most influential top-tier conferences in the field of robotics. In 2025, 1,991 papers (approximately 46.2%) were accepted out of 4,306 submissions, and the conference will be held in Hangzhou, China, from October 19 to 25 (local time). 1) IEEE International Conference on Robotics and Automation The two research papers to be presented by OSX are as follows. …

Topic

2025/05/09

OMRON SINIC X to Present Latest Research Findings at ICRA 2025, Top-tier Conference in the Field of Robotics

OMRON SINIC X Corporation (HQ: Bunkyo-ku, Tokyo; President and CEO: Masaki Suwa, hereinafter “OSX”) will present the latest research findings at the 2025 IEEE International Conference on Robotics and Automation (ICRA 2025) (hereinafter ” ICRA 2025″). ICRA 2025 is one of the world’s largest and most influential international conferences on robotics and automation. In 2025, out of 4,153 submissions, 1,606 papers (approximately 38.67%) were accepted. The conference will be held in Atlanta, United States, from May 19 to May 23, 2025 (local time). The research papers to be presented by OSX are as follows: ICRA 2025 presentations ■ SCU-Hand: Soft Conical …

Topic

2025/04/11

OMRON SINIC X to Present Latest Research Findings at ICLR 2025, Top-tier Conference in the Field of Machine Learning

OMRON SINIC X Corporation (HQ: Bunkyo-ku, Tokyo; President and CEO: Masaki Suwa; hereinafter “OSX”) will present the latest research findings at the Thirteenth International Conference on Learning Representations (ICLR 2025)(hereinafter “ICLR 2025”). ICLR 2025 is one of the top-tier international conferences in the field of machine learning, particularly known for showcasing cutting-edge research in deep learning and representation learning. The conference will be held from April 24 to April 28, 2025, in Singapore (local time). The two research papers to be presented by OSX are as follows. ICLR 2025 presentations ■ Rethinking the role of frames for SE(3)-invariant crystal structure modeling …

Topic

2023/09/04

Introducing Collaborative Research Results with Osaka University Presented at the Leading Robotics Conference “IROS 2022” – Automated Powder Grinding by Robots –

 In this research, we introduce a study on robotic powder grinding for the automation of material science experiments, which was presented at the 2022 IEEE/RSJ International Conference on Intelligent Robots and Systems (IROS).1 This collaborative research is a joint achievement between OMRON SINIC X (OSX) and the Ono Laboratory at Osaka University (called the Graduate University for Advanced Studies at the time the research started). 1: Yusaku Nakajima, Masashi Hamaya, Yuta Suzuki, Takafumi Hawai, Felix von Drigalski, Kazutoshi Tanaka, Yoshitaka Ushiku, and Kanta Ono, “Robotic Powder Grinding with a Soft Jig for Laboratory Automation in Material Science,” 2022 IEEE/RSJ International …

Research

2023/09/04

OSX Research Group Introduction Vol. 1: ROBOTICS Group – Soft Robotics –

   We present a series of articles introducing the OSX Research Group. In the first installment, we provide an overview of the Soft Robotics technology developed by the ROBOTICS Group.  Our goal is to achieve robots capable of performing various tasks, such as component assembly and cooking, in the same space as humans, fostering harmony between humans and machines. Traditional robots have been required to perform predetermined actions quickly and accurately. To execute these predetermined actions, meticulous preparation of the work environment specific to the robot was necessary. However, when working in the same space as humans, it is not …

Research
Page
Top