OMRON developed 3D-LiDAR for front long range with a detection distance of 150 m or more
September 13, 2018
OMRON Automotive Electronics Co., Ltd. (Headquarters: Aichi Prefecture, Komaki City, President: Katsuhiro Wada) announced the global release in September of its 3D-LiDAR* for front long range.
We realized twice the detection distance, 150 m or more, while maintaining the vertical high resolution at the same level which is the characteristic of the around short range 3D-LiDAR announced last October. In addition, in order to improve detection performance in front long range, the horizontal resolution of the central area is doubled.
This increased the ability to recognize not only distant obstacles (four-wheeled vehicles, two-wheeled vehicles, pedestrians, etc.) that are required for autonomous traveling at high speed but also low obstacles (curbs, falling objects, etc.) on the road surface and road surface shapes (inclination, irregularities Etc.) . Classification accuracy is the same as for around short range.
* LiDAR: Light Detection and Ranging, Laser Imaging Detection and Ranging
In addition, this 3D-LiDAR has commonized the product size, internal mechanisms except optical components, and most software with 3D-LiDAR for around short range. This makes possible to consider efficiently the number of mounted 3D-LiDARs and their mounting locations according to the applications of autonomous driving vehicles (AD vehicles) and advanced driver-assistance system vehicles (ADAS vehicles).
3D-LiDAR will contribute to realizing highly reliable automatic driving and advanced driving support suitable for various road environments around the world because it can detect various road surfaces and obstacles in front of the vehicle and around the vehicle essential for autonomous driving with wide field of view and high resolution.
We will continue to work on the development of highly accurate sensing technology and will strive to realize a safe and secure mobility society.
We exhibited the above "3D-LiDAR" at "GTC Japan 2018" held at Grand Prince Hotel New Takanawa International Convention Center Pamir on 13 (Thursday) and 14 (Fri) 2018.
At the venue, you can see a demonstration exhibition using "NVIDIA DRIVE".
Specification
| Product name | 3D-LiDAR | ||
|---|---|---|---|
| Appearance | ![]() |
||
| Use | For front long range | For around short range | |
| Max range |
Object: Reflector | 150m or more | 80m or more |
| Object: Vehicle body | 100m or more | 50m or more | |
| FOV | Horizontal 140° x Vertical 14.4° | Horizontal 140° x Vertical 20° | |
| Resolution | Horizontal 140/280pixel x Vertical 28pixel |
Horizontal 140pixel x Vertical 32pixel |
|
| Size | W124 x H78 x D73.5mm | ||
About OMRON Corporation
OMRON Corporation is a global leader in the field of automation based on its core technology of "Sensing & Control + Think". OMRON's business fields cover a broad spectrum, ranging from industrial automation and electronic components to automotive electronic components, social infrastructure systems, healthcare, and environmental solutions. Established in 1933, OMRON has over 36,000 employees worldwide, working to provide products and services in 117 countries. In the field of industrial automation, OMRON supports manufacturing innovation by providing advanced automation technologies and products, as well as through extensive customer support, in order to help create a better society. For more information, visit OMRON's website at: https://www.omron.com/.
- Contact (media):
- Brand Communications Department
OMRON Corporation
Tel: +81-75-344-7175 - Contact (product information):
- Corporate Planning Department
OMRON Automotive Electronics Co. Ltd.
Tel: +81-568-78-6181