iWnn IME for Web

What is iWnn IME for Web?

A new character input service that supports various situations with Cloud.

A service that provides the highly functional iWnn input engine on the cloud, as a package that includes an IME running on a web app. Supports several different operating systems and browsers, so provides a uniform input environment regardless of the device in use. Includes dictionaries of specialist terminology, enabling input of specialized characters used in various industries.

Product Features

Feature1

Multi-OS / browser support

The keyboard to display can be freely selected to match various text input fields.

An IME supporting several different operating systems and browsers is embedded for use in a web app, enabling input in a wide range of device environments.

Diagram showing iWnn Japanese Input System's multilingual dictionary support, displaying input candidate display functionality for Japanese, Chinese, Korean, English, and French

*Please contact us for details on operational environment.

Operating OS
(checked operating systems only)
Windows10
macOS Catalina
iPadOS(iOS)
Android
Operating browser
(checked browsers only)
Google Chrome ver:84.0.4147.105 (64bit)
Microsoft Edge
Safari

Feature2

Optimum predictive character conversion

Dictionary data is managed on the cloud, providing rapid support for the latest vocabulary and making updates easy.

Dictionaries of specialist terminology are included, reducing the work needed to enter characters. Character input is also assisted by character conversion functions with association prediction and conjunctive phrase conversion.

Medical

Medical dictionary Includes specialist medical terms to enable optimum predictive character conversion.

Medical

Education

Education dictionary Removes inappropriate vocabulary. Selects terms appropriate for the junior high school level, displaying hiragana characters in place of any unfamiliar kanji characters.
Function for displaying/hiding selections Enables unneeded predictive input selections to be hidden when they hinder learning.

Education

Example of Conversion Candidate Control in the iWnn Japanese Input System: Comparing Differences in Conversion Candidates Between Normal Mode and Common Kanji Restriction Mode (for Elementary, Junior High, and High Schools)
Comparison of ON/OFF Settings for the iWnn Japanese Input System's Predictive Conversion Feature: Diagram Explaining Differences in Candidate Display When Inputting 'San-kin Kōtai'

Feature3

Flexible selection of keyboards

The keyboard to display can be freely selected to match various text input fields.

Education

Standard keyboard layouts such as Japanese, Western and flick keyboards can be displayed along with specialized keyboards for entering chemical or numerical formulas.

Keyboard for chemical formulas
Shows only the letters found in chemical formulas used at the junior high school level. Can also be used to enter superscript and subscript characters, enabling flexible input of answers ranging from simple chemical formulas to formulas for chemical reactions.
Keyboard for numerical formulas
Covers the symbols and numerical patterns used at the junior high school level, enabling input of complex numerical formulas.
iWnn Japanese Input System's Chemistry Formula and Mathematical Expression Keyboard for Middle School Students, featuring input support functions tailored to learning content such as chemical reaction formulas and quadratic equations.

PRESS RELEASE

Presents some press releasess of iWnn IME for Web.