menu

OMRON

OMRON Electronic Components Web

Global

Print

Change Text Size

  • S
  • M
  • L

Realizing a highly accurate flow measurement, sensing even a single flap of a butterfly’s wings

Omron’s MEMS flow sensor accurately detects minute airflow so much as a single flap of a butterfly’s wings.

A gas flow sensor capable of “measuring mass flow” independent of temperature and pressure.

高精度 高感度 小型

Mass Flow Measurement

Q1 There are two balloons; each having different volumes. But these balloons have the same mass. Why is that?
A The volume increases/decreases according to the pressure and temperature changes. The mass, on the other hand, remains constant regardless of the environmental changes. The mass flow measurement allows measurement performance that is not affected by the changes in the environment.
Q1 Why is mass flow measurement required?
A An accurate measurement of the flow is required especially for combustion control. Omron’s flow sensor enables measuring the gas flow based on the mass flow measurement.

Principles of MEMS Flow Sensor Measurement

D6F Series

気体の流れがない状態
During the absence of airflow, the temperature distribution around the heater is symmetrical. When there is airflow, the temperature of the upwind side cools down and the temperature of the downwind side warms up, disrupting the symmetry of the temperature distribution.
気体の流れがある状態
By detecting this temperature difference appearing as a difference in the electromotive forces developed by the thermopiles, it allows the mass flow rate and mass flow velocity to be measured without the influence of temperature and pressure. Since the thermopile generates the thermo-electromotive force, the power consumption is much lower than when using the resistivity method.

Highly Resistant to Dust

Built-in Dust Segregation System (cyclonic)

D6F-W/-V/-P

The sensor can be placed anywhere thanks to its dust-resistant structure. Omron’s unique design of 3D flow path provides a high level of reliability by separating dust particles to reduce its effect on the sensor chip. Additionally, Omron succeeded in reducing the sensor size, allowing it to be used in wider range of applications.

耐ダスト構造
外部の流れ

仕様検索

Page Top

Select Your Area
close